Industry Online Support
Technical Forum
4/18/2007 9:16 AM | |
Posts: 1084 Rating: (72)
|
Hi, Haven't tried it yet, but you could look at: Both pc's in same domain? user rights setup oke in IE and IIS and windows. Try running with admin logged in. maybe someone else? with regards, Ikkezelf |
4/18/2007 10:53 AM | |
Joined: 11/23/2005 Last visit: 11/5/2024 Posts: 9 Rating: (0) |
Hi, Both PC's are in same domain. I am administrator on both PCs. I canconnect WinCC/Web Navigator client on client PC to another WinCC server running under Windows 2000, so I think problem is on Windows Server 2003 R2 SP1. I checked IISon both servers and it looks it's the same. SimaticSecurityControl was succesful. On Windows Server 2003 R2 SP1 isalso running another Web (ASP.Net) which isreachablefrom any client. Any hint? Thanks Leo |
4/18/2007 11:20 AM | |
Posts: 3149 Rating: (171)
|
Hi please only use those Software-versions which are mentioned in the compatibility matrix....any other versions (SPs) are not tested and released. => did you have a try with deinstalling SP1? http://support.automation.siemens.com/WW/view/en/21927774 nemo |
Follow us on