Industry Online Support
Technical Forum
1/9/2008 4:06 PM | |
Posts: 4 Rating:
|
Dear reader, I'm experimenting with the WinCC Web Navigator V6.1 SP1running along WinCCV6.0 SP4 HF2. The web browser I use is Internet Explorer 6 SP1.OS is WinXP Pro SP1.I'm using the demo project that came with the Web Navigator installation CD. As explained in the help files, I configured and published this WinCC project as a web site.All mentioned software is running on the same pc.WinCC and Web Navigator are both properly licensed (no demo mode). So far everything works fine. But now, I'mexperiencing a curious problem: Whenconnecting with internet explorer (with Web Navigator Client)to the WinCC project-website ON THE SAME COMPUTER WHERE WINCC SERVER AND WEB NAVIGATORSERVER IS RUNNING, it pops up three errors for every *.pdl file that is loaded. I attached the three errors in zip fileto this thread. I understand from the error messages that internet explorer cannot find some included header files. When via Internet Explorer (and Web Navigator Client)connecting to the WinCC website fromANOTHER pc (also running Win XP Pro SP1), these errors doNOT occur. I find this rather odd (since this is ademo project from Siemens, which I expect to run fine)and wonder what is going on here. Has anybody a clue? Thanx in advance, Kind regards AttachmentCissScriptErr.zip (42 Downloads) |
Follow us on