1/2/2013 2:26 PM | |
Posts: 3 Rating: (0) |
Kindly refer the enclosed system configuration. Attachmentsystem config.pdf (165 Downloads) |
1/4/2013 12:43 PM | |
Posts: 836 Rating: (100)
|
Hi, according to this manual - chapter 4.4 it doesn't seem to be a usual configuration. Configuration with Web diagnostics server and Web diagnostics client (OS single-station system) You use this configuration for an OS single-station system. You can use this configuration to perform cost-effective remote maintenance with one or a few Web diagnostics clients on multiple OS single-station systems/Web diagnostics servers. NOTICE The preferred and standard solution is a configuration with a Web server and Web client. The configuration with Web diagnostics servers and Web diagnostics clients is only intended for plants that have a relatively small number of clients and in which clients connect sporadically to the servers for diagnostic purposes. |
Follow us on