12/5/2008 1:20 AM | |
Posts: 1064 Rating: (72) |
Did you set up a user and password in user adminastration . this should be the user and passsword you need to connect with web navigator |
12/5/2008 10:40 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hello, as playerslight said you have to create the user/password for the "WebUser" in your WinCC Useradmin of your WebServer. But additional you have to pay attention for setting the checkbox Webnavigator and choosinga start picture for this user. You can use a existing user as "WebUser" too. You only must set the checkbox Webnavigator and choosinga start picture for this user too. Cumu |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
12/6/2008 4:11 PM | |
Posts: 1064 Rating: (72) |
Which version of vista are you running, professional or ultimate 32 bit or 64 bit |
12/7/2008 11:25 AM | |
Joined: 2/20/2007 Last visit: 11/24/2024 Posts: 18 Rating: (2) |
this problem apear in: Windows XP EN + SP2 Windows Vista 32 |
12/11/2008 4:19 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hello andrematins2, in this case it would be better to contact the technical support. Because you can not do anything wrong. You only have to do the settings as we wrote above. I think a investigation of your project is necessary. Cumu |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on