4/25/2012 2:04 PM | |
Joined: 12/1/2009 Last visit: 9/5/2024 Posts: 672 Rating: (147) |
Dear RAJKIRAN, search and read aboutSIWAREX. Regards. |
Give us your feedback and show us your respect! |
|
This contribution was helpful to1 thankful Users |
4/25/2012 2:15 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello Rajkiran, You can Used the Siwarex Module In ET200M You have option of Siwarex U & M U is for the Basic One, M is With some more Advance Feature. In Siwarex U you can used 2 Channel or Sinagle Channel Module, In ET200S You have Option of Siwarex CS Is there a demo project for SIWAREX U, FTA, FTC, CS, CF or MS? |
Ammy |
|
This contribution was helpful to1 thankful Users |
4/25/2012 2:46 PM | |
Joined: 8/18/2009 Last visit: 6/17/2024 Posts: 548 Rating: (33) |
thanks to all, Dear Lucky123, could you send me this standard block for load cell.
|
Rajkiran Patil |
|
4/25/2012 3:04 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Ok Siwarexis load cell series as can be seen in attached file. Whereas Rajkiran already has load cell with him which he needs to connect with PLC. @Rajkiran please correct me if Iam wrong
Attachmentsiwarex.pdf (254 Downloads) |
Last edited by: manmeet at: 4/25/2012 3:06 PM |
|
Follow us on