11/30/2015 10:30 AM | |
Posts: 206 Rating:
|
Hi Ron, the best solution for weighing with ET200SP is the Siwarex WP321. http://w3.siemens.com/mcms/sensor-systems/en/weighing-systems/weighing-electronics/plc-based-weighing-modules/Pages/Weighing-module-SIWAREX-WP321.aspx The module can be integrated easily into a S7-1500 system. There are "Ready for use" TIA-Projects for this: https://support.industry.siemens.com/cs/de/en/view/94109373 The Manual you find here: https://support.industry.siemens.com/cs/de/en/view/90893240 The evaluation of the weighing signal you have to do with the PLC. To decide load cell type and mounting units I would need more information about the installation like dead load, length of the conveyor, time to measure, drawing of the conveyor.... See also attached questionnaire. You can send all these data into a support request: https://support.industry.siemens.com/cs/sc/2100/support-request?lc=en-DE
Regards ABenno
AttachmentQuestionnaire_EN.pdf (72 Downloads) |
10/13/2016 3:48 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4792 Rating:
|
New question published by AutoGen_948162 is split to a separate thread with the subject How can i calculate perameter to use third party weight module. Best regards |
Follow us on