8/26/2009 11:36 PM | |
Posts: 3 Rating: (0) |
I am looking for some information and a little direction in a communication option for a client of ours. Currently this client has a 315 PN/DP communicating to three wago remote drops and three VFDs all on profibus and there are three computers with touch screens communicating on profinet. My problem is that this system is on a drilling rig and the comm cables being used are fiber-optics. They are continuely having to replace these cables and proving to be a very costly process. I would like to present a wieless option to them your comments and guidance would be greatly appreciated. Ihave attached a pdf of the system for further clarification. The distances between the buildings are aprox. 75m and are in line of sight.
AttachmentCommunication Layout.pdf (179 Downloads) |
8/28/2009 1:28 PM | |
Posts: 5822 Rating: (412)
|
Hello, |
9/1/2009 8:26 PM | |
Posts: 3 Rating: (0) |
Hello J_Bell, Yes I intend to replace the PROFIBUS as well as the Ethernet Connections |
Follow us on