Industry Online Support
Technical Forum
4/1/2011 9:13 PM | |
Posts: 133 Rating:
|
You will find this in the FH1 function manual for S120. Attached is the section out of the new V4.4 manual. AttachmentPages from FH1_Positioning.pdf (130 Downloads) |
4/2/2011 7:51 PM | |
Posts: 45 Rating:
|
Thanks a lot What parameters must be modified in order to move theservomotor from my PC, with software STARTER? I want to move from PC. / Commissioning / Control Panel /the servomotor for test. STARTER PC image thanks Attachmentimage.pdf (102 Downloads) |
4/3/2011 6:36 PM | |
Joined: 6/4/2008 Last visit: 1/20/2023 Posts: 1414 Rating:
|
Hi, no parameters require changing, that is the point of taking control from the PC. Please see the attached image, you need to click on the LM module button, you should then see the DC Link Precharging, after which the Enables should be available. Cheers, Graeme
AttachmentImage_Pre-Charge.pdf (106 Downloads) |
Follow us on