7/1/2021 3:18 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi vorapob, the Input address is what you projected in the properties of TM_Count. the capture-functionis like a snap-shot of the count-value. its needfull for fast changing signals. It depends on your sensor and its signals how to connect it. SW-gate and capture function don´t depend on each other. But if the SW gate isn´t open (and count value doesn´t change), the capture function is useless. All these information are also content of the device-manual, with a more detailed description: SIMATIC S7-1500 TM Count 2x24VI also recommend this manual: SIMATIC S7-1500, ET 200MP, ET 200SP, ET 200AL Counting, measurement and position detectionhope this helps, regards, |
FCK WAR! |
|