5/15/2018 6:15 PM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating:
|
What is then the right procedure to get all parameters wright after exchanging the powermodule? Do I need to go through the commissioning wizard and select the wright powermodule and that is all (and download off course)? Or is there a parameter in the expert list I can change? Will othere parameters also need to be adjusted for proper functioning? Is f.I. a new autotuning of the motor required when changing to a new (different power) motor module? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/4/2018 1:09:21 PMNew subject after splitting |
|
Follow us on