6/10/2009 6:12 PM | |
Posts: 43 Rating: (0) |
Hello i want to know 1-what is this address 2-how can i use it 3-is this address belonge to I/O area in the memory regards |
6/10/2009 6:27 PM | |
Posts: 1064 Rating: (72) |
That is input word 40 (iw40) . and when you try to use in hardware configuration you would not be able to compile with 2 inputs at the same address |
6/10/2009 6:34 PM | |
Posts: 43 Rating: (0) |
Hello all |
6/10/2009 7:06 PM | |
Posts: 557 Rating: (64) |
hi you can simulate more the one cpu at the same time ,but you have to use S7 PLC-SIM V5.4 SP3. find the link this will help you know the master slave communication.. http://support.automation.siemens.com/WW/view/en/6518822 link for MultiCPU with PLCSIM v5.4 SP3 http://www.plc.net.ru/viewtopic.php?t=10730&highlight=plcsim+++sp3 regards |
Last edited by: Eastern at: 6/10/2009 7:12 PM |
|
Follow us on