8/19/2023 6:00 AM | |
Posts: 2 Rating: (0) |
hello i have to connect a PLC S5 (cpu 115 U ) with a new servo motor & servo drive. I want to choose this servo from siemens brand. what kind and type servo motor & servo drive convenient for connection with PLC S5. detail of old servo motor is : (INDERAMAT brand, 28 NM, 380V, Nmax 4000, brake detail: 14 nm, 24vdc,). pls help me ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/21/2023 05:25:50New subject after splitting |
|
Follow us on