7/13/2021 2:14 PM | |
Joined: 12/7/2016 Last visit: 5/31/2024 Posts: 29 Rating:
|
Hello! We are trying to convert original HMI project with MP370 in WinCC 2008 to project with TP 1500 Comfort in TIA Portal 16 Migration tool 16 was not is not suitable for this task as it was expected So we tried Migration tool 13 + TIA 13 SP2 with trial (!) license As it was expected, conversion was not possible until MP370 was not changed to MP377 in WinCC 2008 It was changed successfully except file path to memory card. Then it was succesfully migrated to am13 Then it was finally migrated from am13 to ap13 with warning "the source project contains one or more disabled animations" Transformation from ap13 to ap16 finishes with error "Exception in client upgrade hook: The project or library possible contains data that cannot be upgraded by the currently installed software" This error emerges in both case. If we are trying to open ap13 in TIA 16 on this step. Or if we are changing HMI device from MP377 to TP1500 in TIA 13. I have two questions: What step is required for autofit screens for new dimension? In TIA 13? In TIA 16? How can we avoid this error? We can't see screens in TIA 13. Because of trial license. Thanks for any help! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/14/2021 08:45:25New subject after splitting |
|
7/13/2021 2:49 PM | |
Joined: 5/12/2006 Last visit: 4/28/2025 Posts: 22604 Rating:
|
define unactive :) |
Follow us on