11/1/2020 9:03 PM | |
Joined: 2/21/2017 Last visit: 2/1/2023 Posts: 7 Rating:
|
Hi all, I have an S110 with a CU305PN control head, i am able to go online with the drive via profinet and Siemens STARTER, i can see all the parameters and values. Is it possible to read via profinet the drive values into a s7-1200 PLC, so i can monitor them via a HMI. I am unsure of what telegrams to use to read certain values out of the S110, i am controlling the drive using the digital I/O only but the IP address is set up in the drive. I anyone could give me help with this i will be very grateful. Ian ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/02/2020 10:58:09New subject after splitting |
|
11/2/2020 11:02 AM | |
Joined: 6/19/2017 Last visit: 2/6/2023 Posts: 6401 Rating:
|
Closed cause question posted twice. The second thread with the subject S7-1200 Profinet to S110 CU305PN comms is published within the conference SINAMICS. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on