10/9/2021 8:32 AM | |
Joined: 9/22/2021 Last visit: 10/19/2021 Posts: 5 Rating: (0) |
hi I recently had some strange problems using iot2050 advance. I downloaded the published _iot2050_example_image_v1.1.1.zip (658,6 MB)(sha-256) file and wrote it to the usb flash drive using win32disk. I also set the sd card's priority boot order. After the SD card is started, the STAT LED green indicator will blink. However, when I access the SD card through putty, the connection times out. I had no problem booting from emMC's system. Thanks for your answer, I use 32GB and 64GB SD cards Best regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/11/2021 10:59:14New subject after splitting |
|
Follow us on