6/21/2018 7:08 AM | |
Posts: 1283 Rating:
|
Believe it or not ixo. What I am telling is true. In LSC, I create a connection with LOGO as client and added S7 device. I didn't change the default TSAP and just kept it as 03.00. Then it is able to communicate. If i change the TSAP with the same configuration as what I did in TIA, the it is not able to write to S7. Am I doing something wrong? Jay ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/21/2018 8:45:20 AMNew subject after splitting |
|
6/21/2018 10:34 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, 03.00 defines a one-sided-connection. but it is not possible to define 03.xx in TIA for the S7-1200 Can you show us a screenshot? What FW-version does your S7-1200 have? As I can see in the TIA-help, S7-1200 with FW1.0 were able to use the TSAP 03.xx There is also a application sample whit S7-1200 and LOGO communication, and it is done like ixo65 described. Application examples for LOGO!hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to
1 thankful Users |
6/21/2018 10:40 AM | |
Posts: 1283 Rating:
|
Here you go ixo. I managed to create a project with TIA V13 for your ease with the same settings i mentioned before. I can get data reading with this setting. Please find the attachment. Thanks, Jay AttachmentTSAP TEST.zip (107 Downloads) |
6/21/2018 10:42 AM | |
Posts: 1283 Rating:
|
Yes in TIA its not possible. But in LOGO i use TSAP settings as 03.00 and in TIA i use 10.01. It communicates data with this settings. Is it normal? Jay |
6/21/2018 11:41 AM | |
Posts: 1283 Rating:
|
I just created for your reference. I can send TIA V15 as well. Anyway sorry about that. Leave it. Jay ...sent from App |
Follow us on