1/18/2018 2:19 PM | |
Joined: 4/6/2015 Last visit: 10/25/2023 Posts: 2 Rating:
|
Please! Someone help me! Using WinCC v7.4 SP1 Does anyone have experience with 8+ Modbus TCP-connections into WinCC? I want to collect VFD data from up to 8 VFD. I am using RS485 to Ethernet converter and configured driver for MODBUS TCP/IP with one Ethernet address and different Slave address(DA), when i am communicating with one VFD then status of driver connection is OK, but when communicating multiple VFD, then status of connection driver showing Disconnected for all except 1 VFD(which is also some time showing disconnected) while i have tested all VFD communicating over MODSCAN at a time with remote TCP/IP connection and found OK. So does anyone have any tips or experience with this solution on this scale? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/19/2018 9:43:59 AMNew subject after splitting |
|
Follow us on