1/16/2018 10:47 AM | |
Posts: 45 Rating:
|
Dear all, I need a help regarding this modbus rtu communication. i had four generators with modbus rs485 connected in multidrop setup. we had an CMTP module added to PLC module ET 200 SP. My problem is during starting am getting communication with all the generators, but when i do a power cycle i am losing communication, what will be the possible reason for the same. is it because of program or i need to enable something. what i had done is i had enabled a counter and whenever the the counter value changes from 1 to 4 . i am enabling one modbus_comm_load and modbus_master_db. isnt what i had done is correct or wrong. Is there any troubleshooting techniques to check the same is there any project sample with communication to 4 slaves.. Thanks and regards Antony ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/16/2018 3:42:37 PMNew subject after splitting |
|
Follow us on