11/11/2015 8:54 PM | |
Joined: 12/29/2008 Last visit: 3/1/2025 Posts: 12 Rating:
|
Hi, I am facing a similar problem. When I try to download a PC Station I get a warning saying that the versions are different (offline/online). In the HW catalog of my project I don't see an older version of OPC Server, I only have one option which is v13.0. In the target PC Station I installed the OPC Server DA that is inside the Tool folder during the installation wizard. I am using in my configuration station TIA Portal v13+SP1+Upd5 (Step7 Pro and WinCC Pro) and in the side of the PC Station WinCC Professional Runtime v13+SP1+Upd5. Hope someone can help. Ty. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/12/2015 10:32:14 AMNew subject after splitting |
|
11/12/2015 9:04 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, I think the station was loaded before with TIA V12. and you have TIA V13. reagards |
FCK WAR! |
|
Follow us on