8/20/2017 5:17 PM | |
Joined: 2/16/2017 Last visit: 10/17/2024 Posts: 9 Rating:
|
Dear TIBI68, Thank you for the work you've done. I have successfully implemented your blocks in one of our machines. It's responsible for sending messages to a large LED display. I also have to implement it in our other machine for the same purpose. Unfortunately I'm unable to compile it in TIA v13 and the other machine's program is only available in TIA cause of the newer HMI panels which are incompatible with STEP7. When I try to compile my project I get an error for MBMA340 (FB34):
Is there any way you can help me? I know you've said you don't use TIA Portal, so maybe you could provide me with source code for this particular block? Any help will be greatly appreciated since we've already made investments in installing the LED display on the other machine. Thanks in advance, Wojtek ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 8/21/2017 7:57:37 AMNew subject after splitting |
|
Follow us on