7/31/2019 12:37 PM | |
Joined: 2/12/2018 Last visit: 11/26/2024 Posts: 224 Rating: (7) |
Hi One more question :) I have a project without OB83 (pull or plug of modules). But when I remove a DI8x24VDC ST from my CPU 1512SP F-1 PN, it dosen't go into STOP mode. In the HELP-MENU it says that it dosen't go into STOP mode if it is a CPU 1512SP-1 PN, but is that also the failsafe CPU? Is this not wrong or have I misunderstood the function? Best regards Azkaban ------------------------------------------------------------------------------------------ |
Last edited by: Azkaban at: 07/31/2019 12:38:55Last edited by: Azkaban at: 07/31/2019 12:44:52Last edited by: Jen_Moderator at: 07/31/2019 13:11:31New subject after splitting Please don't forget to rate :) |
|
Follow us on