11/9/2022 7:42 PM | |
Joined: 8/24/2022 Last visit: 2/25/2025 Posts: 4 Rating:
|
Hello, I tried to use the "Authorization" Property Interface in faceplate, it lets me create this property and use it in any object I want to. I've released the faceplate without any issue, and I've declared the authorization right under the Interface properties on the faceplate call in the screen, but when I compile the project, it says that the data type property doesn't exist. Have anyone solved this issue? There`s something that I need to do to make things work the way I want? I`m using WinCC Unified V17 Update 4. Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/10/2022 10:30:51New subject after splitting |
|
Follow us on