9/29/2022 7:50 AM | |
Joined: 4/2/2019 Last visit: 2/16/2023 Posts: 1 Rating: (0) |
Any info when will it be possible to configure CU320-2 DP with CBE20 as profinet slave in the TIA topology? There should be no difference between the CU320-2 PN and CU320-2 DP with Profinet expansion card when it comes to profinet projects. The fact that this important feature is missing is a very bad. Especially now when we have shortages of electronics and we use whatever is available - but we can't, cause it is not supported in TIA - a tool that was forced on us and that was meant to replace all other commisionning softwares. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_6995909 at: 09/29/2022 07:50:47Last edited by: Jen_Moderator at: 09/29/2022 09:24:08New subject after splitting |
|