6/15/2006 9:41 AM | |
Posts: 18 Rating:
|
Where can I find a manual for modbus communication? |
6/15/2006 12:59 PM | |
Posts: 2 Rating:
|
Dear Mr. Droop see below site: http://www.pacontrol.com in attachment file I sent you a good Modbus manual (I think)! best regard P. Gholami Attachmentmodbus.pdf (707 Downloads) |
6/15/2006 1:06 PM | |
Posts: 18 Rating:
|
Thanks!!! |
6/16/2006 10:51 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi Droop, Please look for the Modbus Master and/or slave driver for the CP341/CP441-2 to the next links: Programming software Modbus Master Loadable driver CP PtP Modbus Master V3.1.3 http://support.automation.siemens.com/WW/view/en/8713784 Handbook MM Loadable Driver for Point-to-Point CPs MODBUS Protocol RTU-Format S7 is Master http://support.automation.siemens.com/WW/view/en/1220184 Programming software Slave Modbus Loadable driver CP PtP Modbus Slave V3.1.4 http://support.automation.siemens.com/WW/view/en/8715908 Handbook MS Loadable Driver CP 441-2 MODBUS Protocol RTU Format S7 is Slave http://support.automation.siemens.com/WW/view/en/1218007 There are also capabilitys for Modbus TCP/IP and also for WinCC Flexible Panels to couple with Modbus TCP/IP. The drivers for STEP7 and the Software are in the Programming software links. You have to buy a dongle for the CP341/CP441-2 to let it work. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
6/16/2006 11:01 PM | |
Posts: 5822 Rating:
|
Thanks Late, I was just on the way looking for these links... [:D] Best regards J_Bell |
9/26/2006 4:04 PM | |
Posts: 47 Rating:
|
Modbus Protocoll http://www.modbus.org/docs/Modbus_Application_Protocol_V1_1a.pdf evtl need to be registered :-) Hela |
9/27/2006 2:40 AM | |
Joined: 5/19/2006 Last visit: 11/29/2023 Posts: 548 Rating:
|
I like this one better [:P] http://www.telemecanique.com/85256D570066CD16/All/852566B70073220C85256752006EA537?Opendocument Dec |
Last edited by: Dec at: 9/27/2006 2:44 AM |
|
Follow us on