11/9/2020 11:38 PM | |
Joined: 9/17/2019 Last visit: 10/9/2024 Posts: 5 Rating: (1) |
This seems pretty straight forward. I'm looking at using the new FCT070 on an upcoming project and wanted to play around with it in TIA Portal before making a decision so took at look at the manual. I have the correct HSP so I can integrate it. But I can't seem to figure out where to actually get ahold/download the new SITRANS Library, does any know where I get it? I would really rather use what they have already done then have to make my own FBs if we decide to use it. Thanks in advance. Oh yeah I am using TIA Portal V16 (Step 7 and Wincc Professional) if that makes a difference. |
Last edited by: Jen_Moderator at: 11/10/2020 10:40:30Optimized link. |
|
2/11/2021 2:18 PM | |
Joined: 2/10/2021 Last visit: 3/16/2023 Posts: 1 Rating: (0) |
We plan to use this technologie as well. But can't find the Librarys to integrate it into TiA V16... Any suggestions? Thx in advance
|
2/15/2021 4:46 PM | |
Joined: 11/22/2016 Last visit: 11/20/2024 Posts: 1 Rating: (0) |
Hi there, Library is available on request, please contact your local Siemens process instrumentation contactperson |
2/24/2021 4:30 AM | |
Joined: 3/28/2010 Last visit: 12/6/2024 Posts: 1095 Rating: (215)
|
Depending on where you are in the world, a process instrument distributor might or might not have any idea what a Sitrans Library is. In the US (where there are very few PCS7's, I only know because the Siemens PCS7 office was 5 miles down the road and I made the acquaintance of the guys there. The catalog sheet with the Sitrans Library order number (7MP2990-0AA00) is at this link: https://support.industry.siemens.com/cs/ww/en/view/109765000 |
Last edited by: Jen_Moderator at: 02/24/2021 10:51:32Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on