10/14/2014 11:22 AM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328) |
Hello, this looks likeSTL code from a S5, butI have no idea what 'F 0.0' can be. see attachment. |
|
|
10/14/2014 4:48 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308)
|
Hello edwin saputra Here is a Description of the Logic : Subtract DW 100 from DW 61 ( of the DB opened Earlier ) . Transfer Result to DW 104 Compare DW 61 and DW 101. ( If DW 61 >= DW 101 ) .AND. Flag F0.0 is HI , then Run Timer T21 for a duration of 5 Sec Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
10/24/2014 12:00 PM | |
Joined: 2/12/2014 Last visit: 5/28/2023 Posts: 158 Rating: (0) |
thank's, but i don't understand about "Flag F0.0 is HI". |
10/27/2014 3:48 AM | |
Joined: 2/12/2014 Last visit: 5/28/2023 Posts: 158 Rating: (0) |
yes, thank's... |
Follow us on