Industry Online Support
Technical Forum
3/20/2008 11:01 PM | |
Posts: 2661 Rating: (279) |
Are you sure the MLFB number for the analog input modules is 6ES5 460-4UB11/12 and not 6ES5 463-4UB11/12? If it is 463, then it can be used with 115U. |
3/21/2008 7:40 AM | |
Joined: 8/24/2006 Last visit: 5/31/2024 Posts: 148 Rating: (9) |
Hi! Yes I'm sure...I know if was 463 it's possible ma the card are 460 Thanks for your interest |
Follow us on