7/21/2019 8:08 PM | |
Posts: 9 Rating:
|
Dear All, I have a similar problem as Dragosvv. I want to connect Win7-32bit PC having Simatic ManagerV5.5 to access PLC program online from Remote IO. If possible I would also like to download the program from Remote IO Location. Remote IO is connected by IM153-2 with Piggyback connector and purple cable. This profibus network is about 300m away from CPU. I wish to know all the devices which can help to connect to CPU using Profibus Network. Shekhar ------------------------------------------------------------------------------------------ |
Last edited by: shek at: 07/21/2019 20:10:15Last edited by: Jen_Moderator at: 07/22/2019 07:30:48New subject after splitting |
|
Follow us on