8/20/2014 4:05 PM | |
Posts: 1 Rating:
|
Very helpful! Thank You! ![]() |
8/21/2014 7:24 AM | |
Joined: 4/22/2010 Last visit: 12/15/2022 Posts: 5697 Rating:
|
Hello, Maybe this FAQ is interesting for you too, it shows the way to copy your HMI project from Step 7 The FAQ is about Wincc Flex, protool is the same thing. After copying you can convert your file, delete the old file from step 7 and integrate the new file. Copying HMI projects integrated in SIMATIC STEP 7 at file level : This function only inserts the operator panel located in an HMI project into a STEP 7 project. If you want to replace an existing HMI station, then the HMI station to be replaced has to be deleted in the SIMATIC Manager. Regards, Marcjan |
Problem solved? |
|
Follow us on