12/28/2022 11:33 AM | |
Joined: 6/1/2020 Last visit: 4/2/2024 Posts: 37 Rating: (0) |
I would like to develop a C# OPC XML DA client to can connect to a MP370 panel that is configured to be a OPC server. I know that this panel only can work as OPC XML DA server because according with the documentation, it uses Win CE and it can't use COM or DCOM interface. I have read this documentation: SYH_OPC_76.pdf - SIMATIC NET: PC software Industrial Communication with PG/PC Volu... - ID: 77376110 - Industry Support Siemens it talks about the library to can develop e client in C# for XML DA and XML UA, but i don't know if it is possible to connect to a XML DA server. Anyway, there are a lot of documentation, perhaps a bit odd, with some examples, but I would like to know, actuaally, which is the best or more recent library. Or which could be a start point, some documentation to start with. Thanks. |
Last edited by: Jen_Moderator at: 12/28/2022 13:14:57Link optimized. |
|
12/29/2022 7:22 AM | |
Joined: 6/19/2017 Last visit: 4/23/2024 Posts: 7952 Rating: (162) |
Closed cause question posted twice. The second thread with the subject Could it be a solution to store the data in a database instead of using CSV files? is published within the conference SIMATIC Panel. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on