1/21/2018 1:01 PM | |
Posts: 2 Rating: (0) |
HI dear . I have a question about Brake and Brake unit in V20 Drives. which model need Brake unit and Which models don't need Brake unit when I want to order . do you have any lists about this that I can using that and choose suitable drive ( the list that I can recognize which on has Brake unit and which one does't have before ordering)? thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/22/2018 11:44:25 AMNew subject after splitting |
|
1/22/2018 9:53 AM | |
Joined: 3/31/2015 Last visit: 11/5/2024 Posts: 175 Rating: (16) |
Dynamic braking unit is integrated in V20s from 7,5kW to 30kW. |
Follow us on