6/9/2019 1:30 PM | |
Joined: 12/16/2016 Last visit: 10/21/2022 Posts: 1 Rating:
|
Hi I am using same S120 drive for positioning system. But my concern is when estop is applied I am dropping OFF3 signal. And it stops with sudden jerk. As my operational speed is 3 m/s. Could you suggest which parameter I should adjust so that if any error comes drive should stop with off3 with limited jerk. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/12/2019 10:52:57New subject after splitting |
|
6/10/2019 4:10 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating:
|
Activate the extended ramp function Generator So you can parametrize smoothing Times for OFF1 and OFF3. |
Follow us on