1/19/2021 10:31 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating: (878) |
Hello, To my knowledge SIMODRIVE 611U can be configured as STANDALONE drive (withput PLC) to control servo motors for speed or positioning application. It has DI/DO as well as AI/AO on board terminal for interface connection. It can be controlled via PROFIBUS with installation of option Profibus module. Please refer SIMODRIVE 611 universal SIMODRIVE 611 universal E, Control Components for Closed–Loop Speed Control and Positioning for more detail information. Also please note, this is discotinued product. In Sinamics apart from S120, V20, V90 are also available but restrication are like, motor power handling, encoder interface, application etc. etc. & V60 with Sinumerik 808D CNC controller. HTH |
Last edited by: PISCEAN 2010 at: 01/19/2021 10:40:37Last edited by: Jen_Moderator at: 01/19/2021 11:39:50Optimized link. |
|
Follow us on