Industry Online Support
Technical Forum
9/3/2014 8:44 PM | |
Posts: 784 Rating: (52) |
Kindly check the following: 1-GSD file is available for use with third party systems " S7_1200 in this case" 2-Is it possible to install GSD file for CP 12XX or CP 15XX into step 7 V5.5? |
9/3/2014 9:30 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Kindly check the following: 1-GSD file is available for use with third party systems " S7_1200 in this case" 2-Is it possible to install GSD file for CP 12XX or CP 15XX into step 7 V5.5? Hello Wago, I have tried 1 hour ago and function, I have in the Hardware catalog, Try and send me the result
|
This contribution was helpful to1 thankful Users |
9/3/2014 10:40 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Kindly check the following: 1-GSD file is available for use with third party systems " S7_1200 in this case" 2-Is it possible to install GSD file for CP 12XX or CP 15XX into step 7 V5.5? Hello Wago, 1-I have installed in STEP v5.5 also 2-For CP 1242-5 (S7 1200) I have already installed in STEP 7 v5.5, for CP 15xxI don't know I never installed, I will try tomorrow. |
This contribution was helpful to1 thankful Users |
9/4/2014 8:54 AM | |
Posts: 784 Rating: (52) |
Thank you Ste39 and kindly inform us with the results. |
9/4/2014 11:11 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello Wago, I tried to install the GSD file (CM 1542-5 and CP 1542-5) the first two of this FAQ PROFIBUS GSD files : SIMATIC - Siemens Industry Online Support ... in STEP7 v5.5 and the installation on the Hardware catalog was successful !!! You should physically try if it works, but I haven'tCM or CP1500 now. |
This contribution was helpful to1 thankful Users |
Follow us on