6/17/2009 11:05 AM | |
Posts: 25 Rating: (1) |
the analog input data type is int. Then why its range is in between 0 to 27648 regards NBR |
6/17/2009 11:18 AM | |
Joined: 4/24/2006 Last visit: 9/13/2024 Posts: 8736 Rating: (1167) |
Dear NBR, Please have a look at manual: http://support.automation.siemens.com/WW/view/en/8859629 See chapter 4 and 5. When there is a overflow or overshoot, you will recognise, because value will be higher then 27648 Best regards, Wizard |
This contribution was helpful to1 thankful Users |
6/17/2009 11:21 AM | |
Joined: 1/4/2008 Last visit: 9/2/2024 Posts: 703 Rating: (96) |
Hello, the discussion is already here. Regards Sydney |
This contribution was helpful to1 thankful Users |
6/17/2009 11:29 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hi, Please find the attachement in that you can find the answer for Analog Value. Ammy AttachmentAnalog Module.pdf (306 Downloads) |
Ammy |
|
6/19/2009 8:46 AM | |
Joined: 9/1/2005 Last visit: 8/12/2024 Posts: 4104 Rating: (195) |
Thread closed, because question is already posted in the thread with the subject How 27648 Analaog Maximum Value ?. within the conference SIMATIC S7-300 / S7-300F. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on