5/10/2017 9:47 AM | |
Joined: 9/30/2016 Last visit: 6/4/2025 Posts: 941 Rating:
|
I copied and renamed an older project as a new project since the functionallity and I/O setup are almost identical. The tagnames have been renamed in both S7 and WinCC (Advanced) and I have downloaded the S7 part to a test controller. When I start simulation of the HMI panel I first get the HMI screens looking OK but they quickly end up with lots of ### instead of the 0 most of them should contain (see attached screenshots). What is wrong and how do I correct it ? AttachmentStrange error.zip (255 Downloads) |
Last edited by: xmnj at: 5/10/2017 10:20:08 AM |
|
5/11/2017 10:15 AM | |
Joined: 8/3/2009 Last visit: 6/23/2025 Posts: 15687 Rating:
|
Hello xmnj Here ist also a faq to a simmilar topic: http://support.automation.siemens.com/WW/view/en/88193789 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
5/17/2017 7:32 AM | |
Joined: 9/30/2016 Last visit: 6/4/2025 Posts: 941 Rating:
|
Thanks ChristophD and Murof
|
Follow us on