9/20/2019 12:16 PM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. On a machine we have a sped (revolutions per minute) that is displayed both on a HMI display and on a LED display. As far as I can see in the logic (in the screenshots) it IS the same value (plus some scaling) that is sent to both places. There is however a problem - when the speed is adjusted (by turning a pot-meter) the value is updated immediately on the HMI display but it is 10-15 seconds delayed on the LED display. Where is this delay introduced and how do I remove the delay? AttachmentUpdate speed.zip (167 Downloads) |