3/4/2020 6:59 AM | |
Joined: 3/11/2015 Last visit: 4/9/2025 Posts: 68 Rating:
|
Yes, I got this information under Help in TIA V14, while I was going through each option to be set under Audit trail including its path. And will check the working of this Archivelogfile function like whether the system message pops up if file transferred and is the 300s timer works and the difference between copy and Move functionality of the file and is the file being moved as CSV format or in Archived one. And i even read that the CSV files are read only and using Hmilogchecktool can detect the tampering of CSV file, but it didn't work when I checked and plus the question if it is read only then why the need of Hmilogchecktool? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/04/2020 12:40:38New subject after splitting |
|
Follow us on