3/9/2022 11:02 AM | |
Joined: 2/17/2020 Last visit: 4/21/2025 Posts: 1250 Rating:
|
Hi Timreed234, Something must have gone wrong with the installation of the component WinCC Professional (TIA Portal) V16. If you go to TIA Portal > Help > Installed Software... is WinCC Professional V16 showing? Also, you may want to try to install the installation DVDs directly from the WinCC Professional (TIA V16) trial link. It is valid for 21 days, but if after that time you have a valid license, you can continue using it. In the following FAQ you will find additional information about this project update process: |
A rating will be well appreciated. |
|
This contribution was helpful to
1 thankful Users |
Follow us on