Industry Online Support
Technical Forum
4/7/2013 8:37 PM | |
Joined: 9/27/2006 Last visit: 2/14/2025 Posts: 12336 Rating:
|
Hello mohamed; A WinAC MP is a soft PLC installed on aa MP 277 hardware platform, and based on Windows CE. Basically, the PLC it mimics is a CPU 315, with a few limitations. For example, it has an integrated Profibus-DP port, but it can only handle 32 Profibus slaves on the bus. So you can use an ET 200S DP-slave without issues, as long as you do not try to connect more than the allowed limit. You will find a lot more information on the WinAC MP on the Siemens Industry Mall and in the Product Support webpages: https://eb.automation.siemens.com/mall/en/WW/Catalog/Products/10038329?tree=catalogtree http://support.automation.siemens.com/WW/view/en/30839259 |
Follow us on