7/13/2017 2:52 PM | |
Joined: 5/12/2006 Last visit: 10/8/2024 Posts: 22399 Rating: (3017) |
Hello, as far i know the 547G have no setting for HPET (same on the Field PG M5). Regards Christoph |
7/13/2017 3:06 PM | |
Posts: 7 Rating: (2) |
Wow. Thats mean WinAc RTX F Can't run on this IPC? It's very hard to understand the compatibility with WinAc RTX F products. I've noticed: PackageswithWinCCRT Advanced,WinCCflexible,WinACRTX andWinACRTX F These packages have been released together with the following SIMATICIPCs.
Maybe avoid this problem? I've this configuration in the TIA Portal... |
Last edited by: PierreonimoTIA at: 7/13/2017 4:25:12 PM |
|
7/13/2017 4:34 PM | |
Joined: 5/12/2006 Last visit: 10/8/2024 Posts: 22399 Rating: (3017) |
Hi, have you looked in the BIOS in the Chipset Configuration, that here reall no HPET entry is available? Christoph |
7/17/2017 1:14 PM | |
Posts: 7 Rating: (2) |
End of this topic, This IPC doesn't work with siemens plc based software. The right choice is the 647D for entry level siemens pc based automation. Everybody can transform the IPC347D or IPC547G basic configuration and more to TwinCat 2 or 3 Runtime with Ethercat bus. This choice about rackable pc installation requirement... To finish, Realy close kind of PC configuration for Siemens plc based software... I think that is not very flexible (for a lot of reason, i agree). I'n't found efficient and clear documentation about the subjet... |
Follow us on