1/14/2013 9:49 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating:
|
Hello, a RTDLL ord DLL is an Output of an Visual Studio Project (VC++, VB, C#) which is created with the WinAC ODK Wizard. With the WinAC ODK Wizard you can create Visual Studio Project which create such an DLL/RTDLL file which can be run on an PC-based Controller. it is compressed and specially created that the PC-based Controller can read in interprete these files. The difference between RTDLL and DLL is that an RTDLL runs in the RealTime Kernel of Interval Zero. The big advantage of an RTDLL file is that is also runs if your windows turns into a blue-screen. I created for you an empty RTDLL with the ODK Wizard and tried it on my system. i registered the RTDLL and used the RTDLL in an simple STEP7 project which only makes a SFB65001 call. And everything works well. I attached the RTDLL for you. Why can't you register an RTDLL? Is there an error message? Have you installed all important software components? nice greetings bigfoot AttachmentC:\WinACTmSrv.zip (719 Downloads) |
Last edited by: bigfoot at: 1/14/2013 2:28 PM |
|
1/15/2013 9:15 AM | |
Posts: 33 Rating:
|
Hi, Im going to create a VM with win2K, maybe i can get it to work there. I'm setting it up now. Cant live with the fact that we did'nt solve it :) |
Follow us on