6/2/2008 1:41 PM | |
Posts: 27 Rating:
|
Problem Summery: The SCADA was running fine since past four years. We have not changed any Hardware or Software. WinCC SCADA Rebooted automatically on following instances. 1) Time 22.08 pm – Date 19th May 2008 2) Time 22.22 pm – Date 16th May 2008 3) Time 11.00 AM – Date 31st May 2008 PC:Manufacturer: Dell CorporationFreeHard Drive Space: 44.8 GBProcessor: Intel 4 CPU 3.00 GhzRAM: 512MB OS: Windows 2000 Version 5.0 SP4 SCADA: WinCC 5.1 SP2 , with 64K RT Licence Simatic Net: Software Version:V6.2 - SP1 Confuigured SCADA Connections: Profibus Speed - 1.5 Mbps DH+ Speed - 57.6 kbps PCI Cards: CP5613 PKTX I have attached following for your Ref. 1. Diagnose Folder 2. RA setup Files 3. S7 Files 4. ALMSR_SP.txt 5. Citamis.str 6. Event Log.txt 7. Event Logs.evt 8. Mini051608-01.dmp 9. System Information.txt Thanks in Advance, KD... AttachmentSCADA PC Information.zip (29 Downloads) |
6/2/2008 11:46 PM | |
Posts: 510 Rating:
|
I ran the mini dump file through WinDbg.exe. I did not have all of the symbols for Win2K, so the output did not contain any more than "Probably caused by : cp5613_wdm.sys ( cp5613_wdm+593f )." I have attached the output from WinDbg in case there is some one more knowledgeable than I am at reading it. You could try updating the driver for the CP5613. If that does not fix the problem you may have a 5613 that is dying. BTW it was very helpful that you provided all of the information in your zip file. Bill Attachmentminidump_output.pdf (31 Downloads) |
6/4/2008 10:16 AM | |
Posts: 27 Rating:
|
Hi Bill, Sorry for replying late and thanksfor your prompt reply and your time. I searched in the PC we could not find the anything like "kernel de***" but locally what ever I felt I have uploaded them. In addition to that I have uploaded all the mini files created in the PC. Hope this is what you are looking for. Thanks again for you kind help. KD... PS: If you specify the path of the Kernel de*** files in your reply, I can upload them. AttachmentMini Dump File & Kernel Files.zip (28 Downloads) |
Last edited by: KD... at: 6/4/2008 10:23 AMFailed to upload the attachment... |
|
6/4/2008 1:55 PM | |
Posts: 510 Rating:
|
I looked at all of the mini dump files: 11 were the 5613 2 were due to kmixer.sys 5/1 and 5/18 1 was due to portcls.sys 5/8 1 was due to the Kernel (ntoskrnl.exe) 5/5 The 5613 started having problems on 2/24 Between 2/24 and 4/20 there were 3 crashes Between 5/1 and 5/31 there were 11 crashes Any crashes are too many, butsomehting changed inthe system in May to accelerate the number of crashes. Were there any significantevents, hardware or software? If every crash was due to the 5613, you would normally conclude the 5613 was the problem. Since there were 4 other crashes, the root casue may not be the 5613. I would reload the driver for the 5613. I would also do a memory check on the RAM in the computer. There aremany programs you can use to test the memory. Here is a link to Microsoft's memory diagnostic test. http://oca.microsoft.com/en/windiag.asp Bill |
Follow us on