3/27/2009 7:34 AM | |
Posts: 9 Rating:
|
There was no new application installation, no modyfications and no sudden power loss |
3/27/2009 8:58 PM | |
Posts: 2661 Rating:
|
May be there is a problem with the memory (hard disk or RAM)? I would try to restore working image or perform a fresh reinstall... |
3/30/2009 7:44 AM | |
Posts: 21 Rating:
|
it seems to be the common problem. here you can find good description what is it and how to catch. ...the operating system telling you that a program has malfunctioned and tried to reference to memory address not existed... it could be broken .CHB file. compare it with the other pc one. it could be some autoupdates of OS installed it could be antivirus when I get into such a "memory problem" I take my vacuum cleaner and clean the dust in PC memory & CPU slots. just as idea - if both pc are similar, you can change hdd and examine for error. then you will understand where the problem is - in HW or Sw. Tima |
This contribution was helpful to
1 thankful Users |
Follow us on