3/20/2019 11:26 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (82) |
Hi Did you see the values in your screen? You can use the tool Diagnosis to see if there is some error and the Log file to analice. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
3/22/2019 6:11 AM | |
Joined: 8/10/2018 Last visit: 4/8/2024 Posts: 9 Rating: (0) |
Values are also not displayed on the screen.
|
3/26/2019 2:40 PM | |
Joined: 8/10/2018 Last visit: 4/8/2024 Posts: 9 Rating: (0) |
This settings are set right now |
4/3/2019 12:16 PM | |
Joined: 8/10/2018 Last visit: 4/8/2024 Posts: 9 Rating: (0) |
The problem returned after several WinCC restarts. Still can not find any solution or an adequate reason. |