5/20/2022 5:56 AM | |
Joined: 5/12/2006 Last visit: 2/3/2023 Posts: 21220 Rating:
|
the marked partsa only simulation and runtime have you select unified ES during the setup? |
5/20/2022 6:46 AM | |
Joined: 5/19/2022 Last visit: 8/3/2022 Posts: 3 Rating:
|
Thanks for your answer. I did select ES. I checked setup again and it says ES is installed. See attached image. |
5/20/2022 6:50 AM | |
Joined: 5/12/2006 Last visit: 2/3/2023 Posts: 21220 Rating:
|
can you install the latest update for wincc V17 ES? if i see correct you have installed ES V17.0 and Unified PC V17.0 UPD 1. Maybe it solved if all SW is on the same Update level? |
This contribution was helpful to
1 thankful Users |
Follow us on