9/1/2020 6:12 PM | |
Joined: 6/7/2018 Last visit: 4/10/2025 Posts: 5 Rating:
|
Hello, I have the same problem on an IPC277E (WIn7 CE) on which WINCC ADVANCED 15 is installed. The system was recently purchased. When you want to change a field, the keyboard appears with a delay of about 5-6 seconds. I would like it to appear immediately ... I can't solve this problem with: https://support.industry.siemens.com/cs/de/en/view/109477784 Do you have another solution? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Mingus73 at: 09/01/2020 18:13:31Last edited by: Jen_Moderator at: 09/02/2020 08:10:39New subject after splitting |
|
9/13/2020 8:09 AM | |
Joined: 7/5/2013 Last visit: 4/29/2025 Posts: 3153 Rating:
|
Hello Mingus, you can download DVD 1 here: SIMATIC STEP 7 and WinCC V15 TRIAL Download With running the exe-file (option: only extraction, no installation) the files are merged and you can browse for the CRL_Check. Regards, Frink |
Pi is exactly three! |
|
Follow us on