3/25/2007 10:34 AM | |
Joined: 11/8/2005 Last visit: 6/5/2024 Posts: 335 Rating: (3) |
Can I connect WinCC to S7-300 with PC_ADAPTER? |
3/26/2007 10:28 AM | |
Joined: 11/8/2005 Last visit: 6/5/2024 Posts: 335 Rating: (3) |
If I want to connect S7-300 to "SIMATIC PC STATION" through MPI network in NETPRO.Which CPs can I put in "PC STATION"? |
3/26/2007 1:58 PM | |
Posts: 1275 Rating: (123)
|
Hi Take a look at this post. It may help out! Best regards, Danielle |
3/27/2007 7:59 AM | |
Joined: 11/8/2005 Last visit: 6/5/2024 Posts: 335 Rating: (3) |
Thank you for your help but Ichecked it and I didn't find anything related to my problem. |
3/27/2007 11:07 AM | |
Posts: 1776 Rating: (95)
|
Hi You can use CP-5611 |
This contribution was helpful to1 thankful Users |
3/28/2007 8:39 AM | |
Joined: 11/8/2005 Last visit: 6/5/2024 Posts: 335 Rating: (3) |
If I want to use PC-ADAPTER instead of CP5611,what should I do? |
3/28/2007 12:33 PM | |
Posts: 1776 Rating: (95)
|
Hi, in NETPRO PC-Adapter is not allowed (possible). But You can do this in PG/PC-Interface settings and in WinCC. April |
3/29/2007 9:06 AM | |
Joined: 11/8/2005 Last visit: 6/5/2024 Posts: 335 Rating: (3) |
So I couldn't use AS-OS Engineering. |
Follow us on