9/30/2015 2:39 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating:
|
Hello ThorirOlafur, you can use profibus with
but it's much easier to use the first combination and connect everything in TIA Portal. Here is an FAQ that explains how to connect WinCC (TIA Portal) to a panel using MPI/Profibus: Which TIA Portal software do you have?
You can use the TIA Selection Tool and/or the Compability Tool to look if your combination of PLC and HMI and other periphery is compatible: If you still want to use STEP 7 V5.5 - here is an application example that explains how to connect WinCC (TIA Portal) with STEP 7 V5.x:
|
Last edited by: H.J. at: 9/30/2015 2:47:42 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to
1 thankful Users |
9/30/2015 5:51 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating:
|
Well, I guess he's right. If you use STEP 7 V5.5 you really should look at the application example I linked last in my previous post.
But while you have STEP 7 Professional V13 SP1 anyway... how about downloading the GSD file of your S7-300 PLC (10th from the top: "CPU315-2AF02.ZIP") I would link you the manual page that shows how to install GSD files but my internet and I don't agree on what to load at the moment
|
Last edited by: H.J. at: 9/30/2015 5:57:59 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
9/30/2015 6:14 PM | |
Posts: 22 Rating:
|
hehe great, thanks again for the response, I will maybe try this out |
9/30/2015 7:06 PM | |
Joined: 5/12/2006 Last visit: 12/8/2023 Posts: 21963 Rating:
|
Hello, GSD is not usefull here because is only for communication configuration for this PLC as i-Slave. And you can't migrate the project from Step7 V5.5 to TIA. The only way you have to couple the S7-300 PLC to a TIA HMI is the device proxy. But for this you must have Step7 V5 and TIA WinCC installed on the same System. More Informations you get here: https://support.industry.siemens.com/cs/ww/en/view/73502293 At the end of the description you will find another Solution for TI V11 (Tag Converter). You can trys this if is working for you. But another way is not possible. Regards Christoph |
This contribution was helpful to
2 thankful Users |
Follow us on