7/28/2020 11:52 AM | |
Joined: 7/10/2017 Last visit: 6/23/2024 Posts: 117 Rating:
|
I know 1 pretty ordinary way of doing it by creating Objects for each positions of the Storage chambers and then make their VISIBILITY on/off based on Uppercar position. But this seems to be very old fashioned approach. Isn't it? And also, here the Hmi gives signals to plc about FILLING CHAMBER No. and REMOVAL CHAMBER No. All calculation about FULL AND EMTY CHAMBERS is done by Hmi...(as per existing program).....PLC just following the command to move the cars to required position for loading and unloading.... Regards, Mr. G M Ansari |
Follow us on